2017-01-24 09:54 AM
I am building a peripheral device that will use an STM32 microcontroller. This peripheral device will communicate with a master/supervisory device over a CAN interface. We have tentatively chosen the STM32F091CC as the controller of the peripheral device. This MCU has a hardware CAN module integrated into it.
I have been reading through documentation on the various CAN protocols and looking through various datasheets and community forums regarding CAN implementation on STM32 microcontrollers.
I am now scared that we chose the wrong microcontroller, since I am having an extremely hard time finding CAN libraries that are written for STM32F0 series microcontrollers. There appears to be a fair amount of CAN library stuff out there for STM32F1 and STM32F2 series, however I don't see anything for STM32F0 series.
For example, there are CANopen stacks for sale for F1,F2, and F4 series microcontrollers that cost about $10,000 and up. The fact that these stacks don't seem to be available for the F0 series worries me.
In my case, I don't need to use a high-level protocol like CANopen, I just need to be able to communicate serially with the master/supervisory device. Incorporating other nodes onto the CAN network can be left to future product development/refinement.
I believe I only need some kind of hardware abstraction layer and limited CAN stack to coordinate communication over the CAN bus. The stack I envision would allow me to receive, transmit, and filter CAN messages.
Having never delved much into the world of microcontroller HAL programming, I am wondering if I should stop the presses and change our selected MCU to a STM32F1 or F2 series.
Does anyone know of an open-source CAN stack that I could use on the F0 series?
#can #stm32f0 #can-bus #f02017-01-24 10:02 AM
>>
There appears to be a fair amount of CAN library stuff out there for STM32F1 and STM32F2 series, however I don't see anything for STM32F0 series.
It is third-party IP, is the implementation really any different on the F0 than the F2/F4?
2017-01-24 11:28 AM
That's what I'd like to know!
2017-01-24 02:34 PM
A review of the registers and the reference manual should give you some insight there. As would the SPL, along with the example I've posted for the F2/F4 CAN interface
STM32F0xx_StdPeriph_Lib_V1.5.0\Projects\STM32F0xx_StdPeriph_Examples\CAN\CAN_Networking\main.c
I'm not actively using the F0 Cortex-M0 parts, or have F0 boards with CAN on them, so not something I'm looking to invest time into. From a cursory scan it looks identical.
Do a merge/diff of the SPL code/examples..
2017-01-24 08:07 PM
Hi,
I am also working with the '091 on CAN
If you need some testing, I may be able to try your stuff on my bear metal os.
how can I enable the FIFO1 ... ?
although I have a 16frame buffer
FIFO1 never gets a frame and I am always missing 4 frames..from 16 exactly, which is odd in itself.
Clive, where did you post the F2/F4 CAN examples ?, I tried to find them.
The example here above from Clive from StdPeriph library only Transmits and receives frames, but is it a network stack ?
2017-01-25 01:22 PM