cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to perform FOTA(Firmware over the air) upgrade while using the ST blueMS app.

Nitish Arora
Associate II

Posted on March 21, 2017 at 08:41

While uploading the binary file, I am unable to flash the code to my stm32l476jgy6 while using the ST BlueMS android app.

The code is uploaded 100 percent but it is not flashed.

Attaching the screenshot for the above problem

Please Help

0690X00000603flQAA.jpg0690X00000603SmQAI.jpg

6 REPLIES 6
raphael declercq
Associate II
Posted on March 21, 2017 at 11:01

Hey,

have you tried to use the MOTENV1_V2.2.0 package by ST?

It is an example that use a FOTA, maybe you can start from this project to build yours
Salvatore Curti
ST Employee
Posted on March 22, 2017 at 15:28

Hi Nitish Arora,

in order to help you, could you tell me:

-) phone/tablet model and related android version?

-) ST BlueMS android app version?

-) what is the binary file that you are uploading?

Again, you are using stm32l476jgy6: NUCLEO or SensorTile?

Regards,

Salvatore Curti.
Posted on March 24, 2017 at 07:03

Yes, I am using the same

Posted on March 24, 2017 at 07:12

I am using coolpad dazen 1 with android kitkat 4.4

I am using the ST BlueMS version 3.3

I am trying to upload the BlueMS2_ST binary file, through OTA, provided in the BlueMicroSystem2

I am using sensor tile

Posted on March 24, 2017 at 14:44

Hi Nitish Arora,

Unfortunately we cannot test the FW with the same smartphone model and with the same android version that you are using.

The problem could be the stack bluetooth (Timeout problem) of the smartphone model.

I suggest: after the FOTA, reset the board but you do not close the BlueMS app; when the board is reconnected, repeat the FOTA (the speed will be less).

The images below show the FOTA with the ASUS Zenfone with android 6.

0690X00000606cyQAA.png
Dilbert K
Senior
Posted on September 26, 2017 at 22:15

I am using 'STM32CubeFunctionPack_MOTENV1_V3.0.0' on SensorTile and have same issue today.

The file I used in Android phone is 'Applications\MOTENV1\Binary\STM32L476RG-SensorTile\MOTENV1_ST.bin'

Is this the right file for OTA purpose ?