2016-12-22 04:22 AM
Section 3.3.3 of the reference manual (RM0008, Rev16) for STM32F10XXX MCUs explains in the register description for FLASH_ACR->LATENCY:
Bits 2:0 LATENCY: Latency
These bits represent the ratio of the SYSCLK (system clock) period to the Flash access time.
000 Zero wait state, if 0 < SYSCLK≤ 24 MHz
001 One wait state, if 24 MHz < SYSCLK ≤ 48 MHz
010 Two wait states, if 48 MHz < SYSCLK ≤ 72 MHz
If I see it correctly, the CMSIS header stm32f103xe.h defines odd bits for this purpose:
#define FLASH_ACR_LATENCY_0 (0x1U << FLASH_ACR_LATENCY_Pos) /*!< 0x00000001 */
#define FLASH_ACR_LATENCY_1 (0x2U << FLASH_ACR_LATENCY_Pos) /*!< 0x00000002 */ #define FLASH_ACR_LATENCY_2 (0x4U << FLASH_ACR_LATENCY_Pos) /*!< 0x00000004 */In previous versions of the header file this wasn't the case, even thought the documentation of these bits appears a bit confusing:
* @file stm32f10x.h
* @author MCD Application Team * @version V3.5.0 * @date 11-March-2011...
#define FLASH_ACR_LATENCY ((uint8_t)0x03) /*!< LATENCY[2:0] bits (Latency) */
#define FLASH_ACR_LATENCY_0 ((uint8_t)0x00) /*!< Bit 0 */#define FLASH_ACR_LATENCY_1 ((uint8_t)0x01) /*!< Bit 0 */#define FLASH_ACR_LATENCY_2 ((uint8_t)0x02) /*!< Bit 1 */Best regards
Peter
2016-12-23 04:12 AM
Hi Peter,
Those code lines are used to define every bit's position in FLASH_ACR register (bit-field LATENCY).
To configure the wait states, you should use the definitions in ''stm32f1xx_hal_flash.h'' file.
If this answers your request,
please click on correct
🙂
.Khouloud.
2017-01-03 05:58 AM
Hi Khouloud,
thanks for your response! I'm still not 100% convinced. Also as bitfield, this definition
#define FLASH_ACR_LATENCY_2 (0x4U << FLASH_ACR_LATENCY_Pos) /*!< 0x00000004 */
would represent bit number two, right? But the reference manual states that bit number one must be set for two wait states.
Best regardsPeter2017-01-05 06:19 AM
Hi Peter,
You should not confuse between ''FLASH_LATENCY_2'' and ''FLASH_ACR_LATENCY_2''.
FLASH_LATENCY_2: is what you should use to configure two latency cycles (2 wait states).
It's the second parameter needed by ''HAL_RCC_ClockConfig'' function.
FLASH_ACR_LATENCY_2: is the bit definition of bit N°2 in the ''FLASH_ACR '' register.
I hope this is clear now.
Regards,
Khouloud.
2017-01-06 01:03 AM
Hi Khouloud,
thanks again! Yes it's clear now. I was just too confused about the definitions in V3.5.0 of the header file which worked differently.
Cheers
Peter