cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-CCA01M1 + X-NUCLEO-IDB04A1 + USBhost

Marco Perciavalle
Associate II
Posted on December 26, 2017 at 12:49

Hi, I have these two shields and I want to integrate their libraries into a code generated by CubeMX where USBhost and FATFS middleware with relative pins are defined. I think that Shields' libraries are available only on their evaluation programs, such as SOUNDTER1_V2.0.0 for CCA01M1, aren't them? So, Are there some rules to follow in order to link these libraries? I use EWARM to develop. The board is F401RE.

Thanks a lot, best regards

#cubemx-project #nucleo-f401 #x-cube-soundter1 #x-cube-cca01m1
0 REPLIES 0