cancel
Showing results for 
Search instead for 
Did you mean: 

Input bias current TS3022

Paul Beijer
Associate
Posted on November 28, 2017 at 12:11

Hello,

I have a question about the TS3022 dual comparators.

The datasheet states an input bias current of 300nA max. over full temperature range.

Compared to similar competitor parts this is almost two orders of magnitude higher.

I was wondering if this specification is correct or should it be pA i.s.o. nA?

Thank you,

Paul

--

1 REPLY 1
Pierre SENNEQUIER
ST Employee
Posted on January 02, 2018 at 10:42

Dear Customer,

  The unit is correct. You can see the typical behavior of the IC fig 12. of the datasheet.

  Best Regards,

  P. 

In order to give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.