cancel
Showing results for 
Search instead for 
Did you mean: 

usbser.sys BSOD(bluescreen) on shut down

Thomas Widmer
Associate II
Posted on January 04, 2017 at 08:15

If i do not disconnect the STM32 Boards serial USB connection to the PC Windows 7 I gets an BSOD on shut down.

4 REPLIES 4
Thomas Widmer
Associate II
Posted on January 04, 2017 at 09:06

Problemsignatur:

  Problemereignisname:    BlueScreen

  Betriebsystemversion:    6.1.7601.2.1.0.256.48

  Gebietsschema-ID:    2055

Zusatzinformationen zum Problem:

  BCCode:    9f

  BCP1:    0000000000000003

  BCP2:    FFFFFA8013BAE060

  BCP3:    FFFFF80000B9A3D8

  BCP4:    FFFFFA801401D640

  OS Version:    6_1_7601

  Service Pack:    1_0

  Product:    256_1

Dateien, die bei der Beschreibung des Problems hilfreich sind:

  C:\Windows\Minidump\010417-6942-01.dmp

  C:\Users\widmert\AppData\Local\Temp\WER-18517-0.sysdata.xml

Lesen Sie unsere Datenschutzbestimmungen online:

 

https://community.st.com/external-link.jspa?url=http%3A%2F%2Fgo.microsoft.com%2Ffwlink%2F%3Flinkid%3D104288%26clcid%3D0x0407

Wenn die Onlinedatenschutzbestimmungen nicht verfügbar sind, lesen Sie unsere Datenschutzbestimmungen offline:

  C:\windows\system32\de-DE\erofflps.txt
Posted on January 04, 2017 at 09:15

BugCheck 9F, {3, fffffa8013bae060, fffff80000b9a3d8, fffffa801401d640}

*** ERROR: Module load completed but symbols could not be loaded for iusb3hub.sys

Probably caused by : iusb3hub.sys
Posted on January 04, 2017 at 09:23

It is not usb hub spesific. I tried it with several USB-Hubs all the same.

All ports gets disabled only the USB port of the STM32 Serial-USB Connect remains active.

Posted on January 04, 2017 at 11:12

Update to latest driver version of the On-board USB Host Controller didn't help.

https://downloadcenter.intel.com/download/22824/USB-3-0-Driver-Intel-USB-3-0-eXtensible-Host-Controller-Driver-for-Intel-8-9-100-Series-and-Intel-C220-C610-Chipset-Family