cancel
Showing results for 
Search instead for 
Did you mean: 

DMA configuration for USART Reception in STM32L152

Ajay Paul
Associate
Posted on January 04, 2017 at 14:41

Hi,

I was trying to configure a DMA for receiving data continuously from USART in STM32L152 Discovery board. I am able to configure the USART TX for DMA. But when i am trying to configure the DMA for RX, even interrupt is also not coming. Can anyone suggest me how to solve this issue . I am  adding the code below.

#include 'stm32l1xx.h'

#include 'stm32l1xx_usart.h'

#include 'stm32l1xx_gpio.h'

#include 'stm32l1xx_rcc.h'

#include 'stm32l1xx_dma.h'

#define USART2_BAUDRATE                 115200  

/**************************************************************************************/

 

void RCC_Configuration(void)

{

  /* --------------------------- System Clocks Configuration -----------------*/

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_DMA1, ENABLE);

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

}

 

/**************************************************************************************/

 

void GPIO_Configuration(void)

{

  GPIO_InitTypeDef GPIO_InitStructure;

 

  /*-------------------------- GPIO Configuration ----------------------------*/

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

 

  /* Connect USART pins to AF */

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2);

}

 

/**************************************************************************************/

 

void USART2_Configuration(void)

{

    USART_InitTypeDef USART_InitStructure;

 

  USART_InitStructure.USART_BaudRate = USART2_BAUDRATE;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

 

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

 

  USART_Init(USART2, &USART_InitStructure);

 

  USART_Cmd(USART2, ENABLE);

}

 

/**************************************************************************************/

 

uint8_t Buffer[]='shokam';

 

void DMA_Configuration(void)

{

  DMA_InitTypeDef  DMA_InitStructure;

 

  DMA_DeInit(DMA1_Channel7);

 

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; // Receive

  DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)Buffer;

  DMA_InitStructure.DMA_BufferSize = (uint16_t)sizeof(Buffer);

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART2->DR;

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

  DMA_InitStructure.DMA_Priority = DMA_Priority_High;

  DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

 

  DMA_Init(DMA1_Channel7, &DMA_InitStructure);

 

  /* Enable the USART Rx DMA request */

  USART_DMACmd(USART2, USART_DMAReq_Rx, ENABLE);

 

  /* Enable DMA Stream Half Transfer and Transfer Complete interrupt */

  DMA_ITConfig(DMA1_Channel7, DMA_IT_TC, ENABLE);

 

  /* Enable the DMA RX Stream */

  DMA_Cmd(DMA1_Channel7, ENABLE);

 

}

 

/**************************************************************************************/

 

void DMA1_Channel7_IRQHandler(void)

{

  /* Test on DMA Stream Transfer Complete interrupt */

  if (DMA_GetITStatus(DMA1_IT_TC7))

  {

    /* Clear DMA Stream Transfer Complete interrupt pending bit */

    DMA_ClearITPendingBit(DMA1_IT_TC7);

 

    USART_SendData(USART2, 'C');

  }

   

}

 

/**************************************************************************************/

 

void NVIC_Configuration(void)

{

  NVIC_InitTypeDef NVIC_InitStructure;

 

  /* Configure the Priority Group to 2 bits */

  NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2);

 

  /* Enable the UART4 RX DMA Interrupt */

  NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel7_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

}

 

/**************************************************************************************/

 

int main(void)

{

  RCC_Configuration();

 

  NVIC_Configuration();

 

  GPIO_Configuration();

 

  USART2_Configuration();

 

  DMA_Configuration();

 

  while(1);

}
5 REPLIES 5
Oliver Beirne
Senior
Posted on January 04, 2017 at 15:06

Hi

ajaypaul2008@gmial.com

I have moved your post to the

https://community.st.com/community/stm32-community/stm32-forum?sr=search&ampsearchId=ce1233ef-d5fc-48ea-b8d1-28e9854d529a&ampsearchIndex=0

which is the best place to ask any product-related STM32 questions.

Thanks

Oli

Posted on January 04, 2017 at 15:22

USART2_Rx is at DMA Channel 6 rather than Channel7, isn't it?

Also

- don't look at the UART registers in debugger, reading data register even in debugger clears the RXNE flag

- don't try to use interrupts and DMA at the same time, they work out of the very same RXNE flag

Posted on January 04, 2017 at 16:59

// STM32 USART2 DMA RX (Tx PA.2, Rx PA.3) STM32L152RE NUCLEO - sourcer32@gmail.com
#include 'stm32l1xx.h'
#include <string.h>
/**************************************************************************************/
void RCC_Configuration(void)
{
 /* --------------------------- System Clocks Configuration -----------------*/
 /* USART2 clock enable */
 RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
 /* GPIOA and DMA1 clock enable */
 RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_DMA1, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
 GPIO_InitTypeDef GPIO_InitStructure;
 /*-------------------------- GPIO Configuration ----------------------------*/
 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; // PA.2 USART2_TX, PA.3 USART2_R
X GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
 GPIO_Init(GPIOA, &GPIO_InitStructure);
 /* Connect USART pins to AF */
 GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);
 GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2);
}
/**************************************************************************************/
void USART2_Configuration(void)
{
 USART_InitTypeDef USART_InitStructure;
 /* USARTx configuration ------------------------------------------------------*/
 /* USARTx configured as follow:
 - BaudRate = 115200 baud
 - Word Length = 8 Bits
 - One Stop Bit
 - No parity
 - Hardware flow control disabled (RTS and CTS signals)
 - Receive and transmit enabled
 */
 USART_InitStructure.USART_BaudRate = 115200;
 USART_InitStructure.USART_WordLength = USART_WordLength_8b;
 USART_InitStructure.USART_StopBits = USART_StopBits_1;
 USART_InitStructure.USART_Parity = USART_Parity_No;
 USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
 USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
 USART_Init(USART2, &USART_InitStructure);
 USART_Cmd(USART2, ENABLE);
}
/**************************************************************************************/
uint8_t Buffer[] = 'The quick brown fox jumps over the lazy dog';
void DMA_Configuration(void)
{
 DMA_InitTypeDef DMA_InitStructure;
 DMA_DeInit(DMA1_Channel6);
 DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; // Receive
 DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)Buffer;
 DMA_InitStructure.DMA_BufferSize = (uint16_t)sizeof(Buffer);
 DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART2->DR;
 DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
 DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
 DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;
 DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;
 DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
 DMA_InitStructure.DMA_Priority = DMA_Priority_High;
 DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
 DMA_Init(DMA1_Channel6, &DMA_InitStructure);
 /* Enable the USART Rx DMA request */
 USART_DMACmd(USART2, USART_DMAReq_Rx, ENABLE);
 /* Enable DMA Stream Transfer Complete interrupt */
 DMA_ITConfig(DMA1_Channel6, DMA_IT_TC, ENABLE);
 
 /* Enable the DMA RX Stream */
 DMA_Cmd(DMA1_Channel6, ENABLE);
}
/**************************************************************************************/
void DMA1_Channel6_IRQHandler(void)
{
 /* Test on DMA Stream Transfer Complete interrupt */
 if (DMA_GetITStatus(DMA1_IT_TC6))
 {
 /* Clear DMA Stream Transfer Complete interrupt pending bit */
 DMA_ClearITPendingBit(DMA1_IT_TC6);
 USART_SendData(USART2, 'C');
 }
}
/**************************************************************************************/
void NVIC_Configuration(void)
{
 NVIC_InitTypeDef NVIC_InitStructure;
 /* Configure the Priority Group to 2 bits */
 NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2);
 /* Enable the USART2 RX DMA Interrupt, per RM0038 */
 NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel6_IRQn;
 NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
 NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
 NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
 NVIC_Init(&NVIC_InitStructure);
}
/**************************************************************************************/
int main(void)
{
 RCC_Configuration();
 NVIC_Configuration();
 GPIO_Configuration();
 USART2_Configuration();
 DMA_Configuration();
 while(1); // Don't want to exit
}
/**************************************************************************************/
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t* file, uint32_t line)
{
 /* User can add his own implementation to report the file name and line number,
 ex: printf('Wrong parameters value: file %s on line %d

', file, line) */
 while (1)
 {}
}
#endif
/**************************************************************************************/�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Ajay Paul
Associate
Posted on January 05, 2017 at 05:29

Thanks

Turvey.Clive.002

and

Waclawek.Jan

for the quick replay. And it is working now. But i am not able to figure out that, what is the significance of Buffer initialization? and Do I need to ensure that, the data which I am sending through uart should be same size as that of initial Buffer size??

Posted on January 06, 2017 at 22:05

You'd really want to pick a buffer that suits your needs, doing DMA RX requires some thought if you are not dealing with a constant stream of data. The case for DMA TX is a lot easier to make, and manage.

I used initialization because it is a lot easier to see in the debugger's memory viewer, and that other examples from which this was culled do both TX and RX in a loop from the same buffer, so what is received is ultimately sent out in a loop. The goal generally with the examples is to make them as simple and illustrative as possible, rather than to solve a more complex use case. If the fundamental concepts are understood they can be extended/applied to more complete systems.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..