2017-02-07 08:10 PM
Hello, I have a question about Standby mode when it wakes up from standby with interrupt or anything which command will
executed
for the example/**** Start ****/
/* Check and handle if the system was resumed from Standby mode */
if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) { /* Clear Standby flag */ __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
}
HAL_GPIO_Write(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
HAL_Delay(500);
HAL_GPIO_Write(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
/*Disable all used wakeup sources: Pin1(PA.0)*/
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
/*Clear all related wakeup flags*/
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/*Re-enable all used wakeup sources: Pin1(PA.0)*/
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
/*Enter the Standby mode*/
HAL_PWR_EnterSTANDBYMode();
HAL_GPIO_Write(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);
HAL_Delay(500);
HAL_GPIO_Write(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
while(1) {
}
/**** End ****/�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Which PA5 or PA6 will be executed first after wake up.
2017-02-08 01:40 AM
Hello,
After standby, the processor will start executing your program from the beginning, like after a reset.
So in your case PA5 will toggle first.
I recommend reading page 162 of
.Best regards,
Max
2017-05-04 04:05 AM
Hi,
Is there a way to make the processor continue the program after a wakeup from standby, just like after a wakeup from STOP mode?Best,
Raphael2017-05-04 06:42 AM
2017-05-04 06:50 AM
Thanks so if I want my RTC tu run continuously after wakeup, i have to use stop instead of standby?
2017-05-04 06:55 AM
RTC is not part of core, so it's not reset unless power is removed.
JW
2017-05-04 07:24 AM
the problem is that when my board restarts, it executes the auto-generated MX_RTC_Init() function, which restart the RTC
:(
2017-05-04 07:28 AM