2018-06-30 09:33 AM
Hi .
I have a custom board with ''stm32f767'' mcu on it and an external sram ''is62wv51216bll-55tli ''.
I have two problem first is when MPU is Disable and i have this config :↓
SCB_EnableICache();
SCB_EnableDCache();
.
.
.
/* FMC initialization function */
static void MX_FMC_Init(void){ FMC_NORSRAM_TimingTypeDef Timing;/** Perform the SRAM1 memory initialization sequence
*/ hsram1.Instance = FMC_NORSRAM_DEVICE; hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE; /* hsram1.Init */ hsram1.Init.NSBank = FMC_NORSRAM_BANK1; hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE; hsram1.Init.MemoryType = FMC_MEMORY_TYPE_SRAM; hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16; hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_ENABLE; hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW; hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS; hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_DISABLE; hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE; hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE; hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_ENABLE; hsram1.Init.WriteBurst = FMC_WRITE_BURST_ENABLE; hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY; hsram1.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE; hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE; /* Timing */ Timing.AddressSetupTime = 15; Timing.AddressHoldTime = 15; Timing.DataSetupTime = 255; Timing.BusTurnAroundDuration = 15; Timing.CLKDivision = 10; Timing.DataLatency = 17; Timing.AccessMode = FMC_ACCESS_MODE_A; /* ExtTiming */if (HAL_SRAM_Init(&hsram1, &Timing, NULL) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }}
Then result will be this ↓ (MY_SRAM_BASE_ADDRESS =0x60000000 as datasheet said ) :
MCU will write to the external sram untill 0x60002577 (usually after reset write until here or a little less)... as you can see i putted a HAL_Delay(1) ms after writing to address if i remove it MCU will write to sram just a little something about 0x60000040 and in both case it generate hard fault error after some writing to sram ( i also am able to read this content).
so does any one has an idea ? what is wrong ? why it can't write in whole of my sram ? why when i delete delay it write less ?
and second problem is when i Enable MPU in first try to writing to sram it generate hardfault error . (MPU config :↓ :(
/* MPU Configuration */
void MPU_Config(void)
{ MPU_Region_InitTypeDef MPU_InitStruct;/* Disables the MPU */
HAL_MPU_Disable(); /**Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.BaseAddress = 0x60000000; MPU_InitStruct.Size = MPU_REGION_SIZE_4MB; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);}
2018-06-30 01:39 PM
Might want to review exactly what the Hard Fault is complaining about. Like F7 DISCO/EVAL boards with working external RAM examples.
Would suggest using
FMC_NORSRAM_TimingTypeDef Timing = {0};
to clear any random stack junk from the structure, and make sure you're filling all the appropriate fields, including any related to size/geometry
2018-07-01 06:46 AM
thank you but did not help that much, hardfault is because of AXI bus error and i don't know why exactly is happening ! the problem is i can write to any address of my external sram but just a couple of byte if i want to write a lot of byte this problem will happen ( in case one MPU disable).
2018-07-01 09:44 AM
2018-07-01 11:00 AM
Yep it was a problem thank you again but now there is another problem ?
look at the result and compare it with the first result in original post ... now i can write to whole sram address continusly but it seems upper byte won't work!(won't write 34 just will write 12 on sram ) but in first example it will write 1234 if you see . so i don't think it has pin problem . do you have any idea ?
2018-07-01 11:21 AM
2018-07-01 11:31 AM
2018-07-01 11:37 AM
Adding multi answers to avoid moderation hold
IS66WV51216EBLL-55BLI
STM32Cube_FW_F7_V1.11.0\Drivers\BSP\STM32F723E-Discovery\stm32f723e_discovery_psram.c
/**
* @brief Initializes the PSRAM device. * @retval PSRAM status */uint8_t BSP_PSRAM_Init(void){ static FMC_NORSRAM_TimingTypeDef Timing; static uint8_t psram_status = PSRAM_ERROR;/* PSRAM device configuration */
psramHandle.Instance = FMC_NORSRAM_DEVICE; psramHandle.Extended = FMC_NORSRAM_EXTENDED_DEVICE;/* PSRAM device configuration */
/* Timing configuration derived from system clock (up to 216Mhz) for 108Mhz as PSRAM clock frequency */ Timing.AddressSetupTime = 9; Timing.AddressHoldTime = 2; Timing.DataSetupTime = 6; Timing.BusTurnAroundDuration = 1; Timing.CLKDivision = 2; Timing.DataLatency = 2; Timing.AccessMode = FMC_ACCESS_MODE_A;psramHandle.Init.NSBank = FMC_NORSRAM_BANK1;
psramHandle.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE; psramHandle.Init.MemoryType = FMC_MEMORY_TYPE_SRAM; psramHandle.Init.MemoryDataWidth = PSRAM_MEMORY_WIDTH; psramHandle.Init.BurstAccessMode = PSRAM_BURSTACCESS; psramHandle.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW; psramHandle.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS; psramHandle.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE; psramHandle.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE; psramHandle.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE; psramHandle.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE; psramHandle.Init.WriteBurst = PSRAM_WRITEBURST; psramHandle.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE; psramHandle.Init.PageSize = FMC_PAGE_SIZE_NONE; psramHandle.Init.ContinuousClock = CONTINUOUSCLOCK_FEATURE;/* PSRAM controller initialization */
BSP_PSRAM_MspInit(&psramHandle, NULL); /* __weak function can be rewritten by the application */ if(HAL_SRAM_Init(&psramHandle, &Timing, &Timing) != HAL_OK) { psram_status = PSRAM_ERROR; } else { psram_status = PSRAM_OK; } return psram_status;}&sharpdefine PSRAM_DEVICE_ADDR ((uint32_t)0x60000000)
&sharpdefine PSRAM_DEVICE_SIZE ((uint32_t)0x80000) /* SRAM device size in Bytes *//* &sharpdefine SRAM_MEMORY_WIDTH FMC_NORSRAM_MEM_BUS_WIDTH_8*/
&sharpdefine PSRAM_MEMORY_WIDTH FMC_NORSRAM_MEM_BUS_WIDTH_16&sharpdefine PSRAM_BURSTACCESS FMC_BURST_ACCESS_MODE_DISABLE
/* &sharpdefine PSRAM_BURSTACCESS FMC_BURST_ACCESS_MODE_ENABLE*/&sharpdefine PSRAM_WRITEBURST FMC_WRITE_BURST_DISABLE
/* &sharpdefine PSRAM_WRITEBURST FMC_WRITE_BURST_ENABLE */&sharpdefine CONTINUOUSCLOCK_FEATURE FMC_CONTINUOUS_CLOCK_SYNC_ONLY
/* &sharpdefine CONTINUOUSCLOCK_FEATURE FMC_CONTINUOUS_CLOCK_SYNC_ASYNC */2018-07-02 10:15 AM
the connection are right is just 19 address and 16 data pin and some cmd pin im sure about it . there would be something else when i put these value :
Timing.AddressSetupTime = 0;
Timing.AddressHoldTime = 0; Timing.DataSetupTime = 2;and turn of the mpu i can write to sram for something about 3000 byte with valid data but when i change this parameter everything will corrupt and also with these value i also am able to write just 3000 byte by valid data then it will corrupt again .
2018-07-02 10:19 AM
why pin address 18 is connected to ground in this SCH ? in my Schematic it is connected to MCU as IS62SRAM data sheet said . (actually didn't see anything about connect this pin to ground or other note about pins . )