2018-01-31 12:04 AM
HI.
I am testing with ST Discovery LoRa Kit, PingPong.
There is no problem sending / receiving 64 bytes.However, the size of 64 bytes or more can not be transmitted or received.Semtech says that 128 bytes are possible, but why not?Solved! Go to Solution.
2018-01-31 10:40 AM
I think the issue as observed here is the rejection of large packets where the receiver could be distracted from reception by large corrupt packets. The size is in the header burst as I recall.
The use case for the radio could be small control channel packets, where the radio only keys on these packets and the micro stays in deep sleep states ignoring larger bulk packets not destine for it.
The radio software in the LRWAN explicitly configures the default max to 64 bytes, although this may be changed later programmatically.
{ MODEM_LORA, REG_LR_PAYLOADMAXLENGTH, 0x40 }
2018-01-31 01:57 AM
2018-01-31 08:42 AM
Note that the maximum size of packet depends on the the data rate you're using; eg,
for the European 863-870MHz band, the
applicationpacket size varies between 51 bytes for the slowest data rate, and 222 bytes for faster rates.2018-01-31 10:40 AM
I think the issue as observed here is the rejection of large packets where the receiver could be distracted from reception by large corrupt packets. The size is in the header burst as I recall.
The use case for the radio could be small control channel packets, where the radio only keys on these packets and the micro stays in deep sleep states ignoring larger bulk packets not destine for it.
The radio software in the LRWAN explicitly configures the default max to 64 bytes, although this may be changed later programmatically.
{ MODEM_LORA, REG_LR_PAYLOADMAXLENGTH, 0x40 }
2018-02-01 02:02 AM
Hi Clive One
Thank you for your reply.
I have modified the REG_LR_PAYLOADMAXLENGTH value and it seems to be receiving to some extent. If it is set to 0x80 (128) byte, it will be received only up to about 115 bytes.If 0x100 (256) byte is set, no reception is possible.I need to know only this information.2018-02-01 06:23 AM