2017-08-02 01:52 AM
Hello there.
I am currently developing a coin cell powered device with the STM32L051C8. The datasheet says in standby mode the consumption is about 0.27uA (270nA). My current board only consists of a Voltage Regulator which is rated to max. 300nA self consumption. So the optimum consumption for my device should be around 570-600nA. My current board has consumption of around 800-900nA. So my question: is there a option to optimize the current consumption on software side beside the standard standby entering procedure.
// Enter STBY Mode function.
void HW_EnterLowPower() {
hal_deinit();
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
HAL_PWR_EnterSTANDBYMode();
}
Thanks in advance,
kind regard, Rob.
#standby #stm32l0 #low-powerSolved! Go to Solution.
2017-08-02 03:20 AM
Hello,
I recommend you to look to the PWR
Current Consumption
examples within STM32CubeL0:S TM32Cube_FW_L0_V1.9.0\Projects\STM32L073Z_EVAL\Examples\PWR\PWR_STANDBY
/* The voltage scaling allows optimizing the power consumption when the device is
clocked below the maximum system frequency, to update the voltage scaling value
regarding system frequency refer to product datasheet. */
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
Have a look to
theRegards
Imen
2017-08-02 03:17 AM
Make sure RTC, IWDG, LSE, LSI are disabled. Configure the pins in analog input mode. If possible decrease the voltage coming to VDD at least to 1.8V (or down to 1.65V), use the voltage range 3 for VCORE (1.2V). The PVD, POR and PDR are also eating some current. Refer to the datasheet and
http://www.st.com/resource/en/application_note/dm00108286.pdf
.2017-08-02 03:20 AM
Hello,
I recommend you to look to the PWR
Current Consumption
examples within STM32CubeL0:S TM32Cube_FW_L0_V1.9.0\Projects\STM32L073Z_EVAL\Examples\PWR\PWR_STANDBY
/* The voltage scaling allows optimizing the power consumption when the device is
clocked below the maximum system frequency, to update the voltage scaling value
regarding system frequency refer to product datasheet. */
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
Have a look to
theRegards
Imen
2021-06-24 02:32 AM
@Imen DAHMEN I have followed the standby PWR example but I got 10 mA consumption in standby mode. Here is my code:
void Enter_Standby_Mode(void)
{
//Disable the RTC alarm external interrupt
HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A);
/* Check and handle if the system was resumed from StandBy mode */
if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
/* Clear Standby flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
}
GPIO_InitTypeDef GPIO_InitStructure = {0};
/* Enable GPIOs clock */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
GPIO_InitStructure.Pin = GPIO_PIN_All;
GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;
GPIO_InitStructure.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOD, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOH, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOE, &GPIO_InitStructure);
/* Disable GPIOs clock */
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOD_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
__HAL_RCC_GPIOE_CLK_DISABLE();
/* The Following Wakeup sequence is highly recommended prior to each Standby mode entry
mainly when using more than one wakeup source this is to not miss any wakeup event.
- Disable all used wakeup sources,
- Clear all related wakeup flags,
- Re-enable all used wakeup sources,
- Enter the Standby mode.
*/
/* Disable all used wakeup sources*/
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
/* Re-enable all used wakeup sources*/
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 20, RTC_WAKEUPCLOCK_CK_SPRE_16BITS);
/* Clear all related wakeup flags */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_SuspendTick();
/* Enter the Standby mode */
HAL_PWR_EnterSTANDBYMode();
}