cancel
Showing results for 
Search instead for 
Did you mean: 

Powermanagement using SPC5studio

Santhamurthy R
Associate II
Posted on February 09, 2017 at 07:01

Hello All,

I am new to SPC environment. I am trying to do the configurations for the power management. I am using SPC5studio version 5.2.1, I am not finding the settings to configure the modes (e.g RUN Mode 0, HALT mode, STOP mode, etc) in the application wizard so that I couldn't able to auto generate the code using code generator.

I am working on SPC560B54L5 evaluation board, kindly suggest the steps to generate the code for power management using code generator.

If any ready to use code please update.

Thanks in Advance..

----

Best Regards,

R.Santhamurthy
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee
Posted on February 09, 2017 at 17:53

Hello 

R.Santhamurthy ,

You can not configure R

UN Mode 0, HALT mode, STOP mode, STANDBY mode by the configurator.

Anyway , you can use some application example as example.

SPC560Dxx OS-Less WKPU LPM Test Application for Discovery

SPC560Dxx_RLA WKPU API Test Application for Discovery

you should respect the figure 72 of RM0037

      Best regards

               Erwan

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee
Posted on February 09, 2017 at 17:53

Hello 

R.Santhamurthy ,

You can not configure R

UN Mode 0, HALT mode, STOP mode, STANDBY mode by the configurator.

Anyway , you can use some application example as example.

SPC560Dxx OS-Less WKPU LPM Test Application for Discovery

SPC560Dxx_RLA WKPU API Test Application for Discovery

you should respect the figure 72 of RM0037

      Best regards

               Erwan