cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX: what kind of discovery board is meant?

Dmitrij Rajkov
Associate II
Posted on April 23, 2017 at 21:13

I wanted to create a project for STM32F407G-DISC1 board (STM32F4DISCOVERY?) but saw two identical lines in the selection dialog (see attach).

What kind of discovery board is meant? Or is t

his mistake?

STM32CubeMX 4.20.1.

#stm32f4discovery #stm32cubemx #discovery
2 REPLIES 2
Posted on April 24, 2017 at 01:04

These are equivalent

STM32F407G-DISCO

STM32F407G-DISC1

STM32F4DISCOVERY

The DISC1 has the larger STM32F103 for the ST-LINK, supporting the mbed firmware

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Max
ST Employee
Posted on April 24, 2017 at 05:03

They are the same except for the embedded STLink version (V2: debug only or V2-1: debug, virtual COM port, mass storage).

You can see that by clicking the 0690X00000603VdQAI.jpgbutton.

BR

Max