cancel
Showing results for 
Search instead for 
Did you mean: 

Use CubeMX with BlueNRG-2

A Bravos
Associate III
Posted on August 15, 2017 at 11:17

Hi.

Is it possible to use cubemx with BlueNRG-2? If yes how? Where to find code examples for this microcontroller, with interest for Bluetooth BLE. 

I want to start exploring this Upc and I needed information

.

Thank you. Bravos

2 REPLIES 2
Amel NASRI
ST Employee
Posted on August 15, 2017 at 15:28

Hi

Bravos.A

‌,

CubeMX is dedicated for STM32 MCUs. What is exactly your requirement here?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on August 15, 2017 at 17:10

 ,

 ,

Hi Amel,

Thanks for the answer.

I need to make a low energy application with bluetooth communication and

work with, some i2c and spi sensor readings, with few gpios and that is

ultra miniature, to work at 3.3 volts. As I know the CubeMx, because I

worked with the Discovery board, it would be interesting this aid, to

bootloader setup.

I have never worked directly with bluetooth Ic, and so looking for

information.

Bravos

2017-08-15 14:29 GMT+01:00 Amel N <,st-microelectronics@jiveon.com>,:

STMicroelectronics Community

<,https://community.st.com/?et=watches.email.thread>,

Re: Use CubeMX with BlueNRG-2

reply from Amel N

<,

MCUs Forum* - View the full discussion

<,https://community.st.com/0D70X000006SqoHSAS