cancel
Showing results for 
Search instead for 
Did you mean: 

STPM3x Evaluation Software - Read Buffer Length Insufficient

Rob Parsons
Associate II
Posted on February 15, 2017 at 16:29

Hello,

I have an EVALSTPM34 board.

I am trying to access the board via the UART using the 'STPM3x Evaluation Software' v3.1.0.0

J7 has 3.3v supply attached. 

J2 has TTL-232R-3V3 cable attached.

PC recognizes the TTL-232R-3V3  as COM5.

J3 jumper is removed.

SW1 has all SWs in ON position.

I start up the STPM3x Evaluation Software.

Options > Interface = USRT, COM5, 9600

I press 'Open' and get success.

Options > Configuration > Application tab = EVAL-STPM34

I press 'Apply' and get a pop-up dialog box that says:

Read buffer lenght insufficient.   < Yes, 'length' is mis-spelled.

The operation has timed out.

Has anyone had a similar experience?

Is there a newer version of the 'STPM3x Evaluation Software' ?

Rob Parsons

Schneider Electric

Knightdale NC USA

5 REPLIES 5
Rob Parsons
Associate II
Posted on February 17, 2017 at 14:25

J7 and J2 on the EVALSTPM34 board must both have 3.3v supply attached when using the UART.

Posted on March 18, 2017 at 09:35

Parsons.Rob

I tried to connect the EVAL-STPM32 board to the STPM3x Evaluation Software but encountered the following error when trying to read data.

Error message: 'Read buffer length insufficient. The operation has timed out.'

PC was running Windows 7

STPM3x Evaluation Software v3.1.0.0

In the 'Options -> Interface' menu, the following values were used: UART / COM 5 / 9600 (baud rate)

The board was connected to the PC through a USB to UART Bridge (Silicon Labs CP210x).

J2 connected to the USB-to-UART bridge

J7 connected to an external DC supply of 3.3V

J2 connected to a different 3.3V source

J3 jumper was removed

SWC1 DIP switch was all in on position

J4 jumper was in 'enable' position

I really appreciate your help.

Emanuel A
Associate
Posted on February 15, 2018 at 19:42

Hello! Was there any success in solving this issue? I have the same problem! Please help! Thank you

Posted on May 25, 2018 at 09:27

HI , can u say what changes u did

kaziz anass
Associate

Hey,

I faced the same problem. If you are using RS232, be sure that the Tx (of the board) is connected to Rx (of the cable), and Rx (of the board) is connected to Tx (of the cable). That was a solution for me 🙂