cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 ISR source

Dick Lin
Senior
Posted on May 07, 2018 at 18:26

Hi,

Is there any doc mention about STM32L4 (STM32L4996 and STM32L4A6) ISR source? The doc I found from both ST and ARM reference manual do seems list all of the ISR source.

Thanks,

****

Note: this post was migrated and contained many threaded conversations, some content may be missing.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on May 07, 2018 at 18:32

Hard to decipher

http://www.st.com/content/ccc/resource/technical/document/reference_manual/02/35/09/0c/4f/f7/40/03/DM00083560.pdf/files/DM00083560.pdf/jcr:content/translations/en.DM00083560.pdf

 

See pg 396 of RM0351 Rev 6, Table 57 'Vector Table'

The 'position' field indicates the ISR managed by the NVIC

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

12 REPLIES 12
Posted on May 07, 2018 at 18:32

Hard to decipher

http://www.st.com/content/ccc/resource/technical/document/reference_manual/02/35/09/0c/4f/f7/40/03/DM00083560.pdf/files/DM00083560.pdf/jcr:content/translations/en.DM00083560.pdf

 

See pg 396 of RM0351 Rev 6, Table 57 'Vector Table'

The 'position' field indicates the ISR managed by the NVIC

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 07, 2018 at 18:49

Hi Clive,

Got it. Thanks.

Is there any .h file already define all of those ISR number?

Thanks,

Dick

On Mon, May 7, 2018 at 9:34 AM, Clive One <st-microelectronics@jiveon.com>

Posted on May 07, 2018 at 18:53

STM32Cube_FW_L4_V1.11.0\Drivers\CMSIS\Device\ST\STM32L4xx\Include\stm32l4a6xx.h

Via

STM32Cube_FW_L4_V1.11.0\Drivers\CMSIS\Device\ST\STM32L4xx\Include\stm32l4xx.h

and define STM32L4A6xx on compiler command line

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 07, 2018 at 19:00

Got it. Thx

On Mon, May 7, 2018 at 9:55 AM, Clive One <st-microelectronics@jiveon.com>

Posted on May 07, 2018 at 19:40

Hi,

Is there any example code to manipulate ISR such as trigger, set pripority,

on/off...etc?

Thanks,

Dick

Pavel A.
Evangelist III
Posted on May 08, 2018 at 01:07

Open the project in the IDE (Keil or whatever you have). Build the project.

Then right click on the identifier and select 'go to definition'.

The demo projects should build without any errors. Unless you open the project in a wrong IDE or there's some problem with installation of the IDE.

-- pa

Posted on May 07, 2018 at 23:23

Might I suggest you review Joseph Yiu's Essential Cortex-M3/M4 book and chapters related to NVIC. Settings for Group Priority, and Preemption being of particular importance.

Please review also the assorted HAL examples provided under the repository trees. Use a 'File Manager' to search and view file content.

STM32Cube_FW_L4_V1.11.0\Projects\NUCLEO-L496ZG\Examples\GPIO\GPIO_EXTI\Src\main.c

STM32Cube_FW_L4_V1.11.0\Drivers\STM32L4xx_HAL_Driver\Inc\stm32l4xx_hal_cortex.h

/** @defgroup CORTEX_Exported_Functions_Group1 Initialization and Configuration functions

  * @brief    Initialization and Configuration functions

  * @{

  */

/* Initialization and Configuration functions *****************************/

void HAL_NVIC_SetPriorityGrouping(uint32_t PriorityGroup);

void HAL_NVIC_SetPriority(IRQn_Type IRQn, uint32_t PreemptPriority, uint32_t SubPriority);

void HAL_NVIC_EnableIRQ(IRQn_Type IRQn);

void HAL_NVIC_DisableIRQ(IRQn_Type IRQn);

void HAL_NVIC_SystemReset(void);

uint32_t HAL_SYSTICK_Config(uint32_t TicksNumb);

/**

  * @}

  */

/** @defgroup CORTEX_Exported_Functions_Group2 Peripheral Control functions

  * @brief   Cortex control functions

  * @{

  */

/* Peripheral Control functions ***********************************************/

uint32_t HAL_NVIC_GetPriorityGrouping(void);

void HAL_NVIC_GetPriority(IRQn_Type IRQn, uint32_t PriorityGroup, uint32_t* pPreemptPriority, uint32_t* pSubPriority);

uint32_t HAL_NVIC_GetPendingIRQ(IRQn_Type IRQn);

void HAL_NVIC_SetPendingIRQ(IRQn_Type IRQn);

void HAL_NVIC_ClearPendingIRQ(IRQn_Type IRQn);

uint32_t HAL_NVIC_GetActive(IRQn_Type IRQn);

void HAL_SYSTICK_CLKSourceConfig(uint32_t CLKSource);

void HAL_SYSTICK_IRQHandler(void);

void HAL_SYSTICK_Callback(void);
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 07, 2018 at 23:46

Yes, I am reading the HAL user's manual. I saw those functions you

mentioned in the email.

One more question - is there any functions to set/get M4 register value?

Thanks,

Dick

On Mon, May 7, 2018 at 2:23 PM, Clive One <st-microelectronics@jiveon.com>

Posted on May 07, 2018 at 23:53

Which registers specifically?

Many peripheral and NVIC registers are mapped into memory so are accessible using normal read/write variables, or pointers.

The processor registers (ie R0..R15) would be better accessed via assembler code or inlined as they are nominally used for parameter passing to/from C functions and to hold intermediate values in computations.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..