cancel
Showing results for 
Search instead for 
Did you mean: 

DCMI + FMC on STM32F7

Matthew Lai
Associate III
Posted on March 08, 2017 at 17:57

Hello!

From a cursory glance at the datasheet it seems like there are many pin conflicts between DCMI and FMC on the F7. Does that mean they cannot be used at the same time?

Isn't that a bit of an oversight, considering image data often take quite a bit of memory?

Thanks

Matthew

1 ACCEPTED SOLUTION

Accepted Solutions
Posted on March 08, 2017 at 18:05

Perhaps, it depends on how many pins your chosen device has, and the may be overlap or alternate options. Historically some of the AF muxing choices had been a bit brain damaged. (SDIO or ETHERNET vs LCD on the STM32F429I-DISCO)

Haven't done the due diligence on the pins here, does CubeMX provide escape on the maximal pin product?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2
Posted on March 08, 2017 at 18:05

Perhaps, it depends on how many pins your chosen device has, and the may be overlap or alternate options. Historically some of the AF muxing choices had been a bit brain damaged. (SDIO or ETHERNET vs LCD on the STM32F429I-DISCO)

Haven't done the due diligence on the pins here, does CubeMX provide escape on the maximal pin product?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 08, 2017 at 18:25

Ahh yes of course. Had a brain fart, thanks!

Forgot they can be on multiple pins!