cancel
Showing results for 
Search instead for 
Did you mean: 

Can the L6615 load share controller be used for 50V bus high side application? A resistor divider to reduce common mode can be used on the sense pins but how do you calculate the component values?

Bill Drumheller
Associate
Posted on February 18, 2017 at 17:51

I am using the L6615 in a 50V bus current sharing application and I have the required voltage divider from each side of the high side current sense resistor to ground but I am unsure if another series resistor needs to be placed in series with the sense pins on the IC.  Any guides on how to calculate these values would be appreciated.  Thanks!

0 REPLIES 0