cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-1 run debug, combine with cc1310

Nav Dev
Associate II
Posted on February 23, 2017 at 13:00

Hi ST,

I am working with the BlueNRG-1 using STEVAL_IDB and i have few questions please:

1- When i program some ST BLE via using Navigatorv2.3.0, the main code not the BLE stack, where it saved? in the main MCU or the NRG-1?

2- I want to combine the NRG-1 with TI sub1-GHZ cc1310(Backward compatibility), so i have few questions in this area:

2.1 - Where the code that related to the BLE must run? on the cc1310 or NRG-1?

2.2 - Did it possible to configure and send commands to the NRG-1 via other MCU? if yes i would be happy if you share some example, reference ...

3- Did there is some tool develop/debug with the 

BlueNRG-1 code example, and it's free?

4- What is the best IDE that you recommended to work with the BlueNRG-1?

Thanks.

#bluenrg-1
2 REPLIES 2
Imen.D
ST Employee
Posted on February 23, 2017 at 16:21

Hi,

You may refer to the User manualsand related Tools/softwarein the

http://www.st.com/content/st_com/en/products/wireless-connectivity/bluetooth-bluetooth-low-energy/bluenrg-1.html

.

The BlueNRG GUI is available in

/external-link.jspa?url=https%3A%2F%2Fmy.st.com%2Fcontent%2Fmy_st_com%2Fen%2Fproducts%2Fembedded-software%2Fwireless-connectivity-software%2Fstsw-bnrgui.license%3D1487062354html

.

Hope this helps you.

0690X00000606F2QAI.png

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on March 08, 2017 at 11:00

Thanks 

Imen D for responding, 

After looking to the references that you advice to me, i have few question please:

As i mentioned before, we want to use TI cc1310 for SUB1-GHz and the NRG-1 for BLE, there is 2 ways (that i know about):

1- Connect the NRG-1 to the cc1310 via SPI and send ACI commands.

2- Set the NRG-1 as a Stand Alone, and share some memory between the cc1310 and the NRG-1 for logic's and others...

Q1: did the ACI commands have full control of the BLE stack as the Stand Alone?

Q2: What is the best way, the first way or the second?

Q3: Did there is another way that o didn't mentioned?

Any other advice in this topic will be welcome.