cancel
Showing results for 
Search instead for 
Did you mean: 

How to detect click/double click with LSM9DS1

Xiangfan Lee
Associate
Posted on February 27, 2017 at 08:17

Hello everyone,

In the data sheet of LSM9DS1, it is stated in the first page that the device supports:

  • Position and motion detection functions

  • Click/double-click recognition

However I cannot find anywhere in the data sheet describing how to use the features?  Could someone help me on this? Thanks a lot!

#lsm9ds1-click-detection
2 REPLIES 2
Miroslav BATEK
ST Employee
Posted on February 27, 2017 at 10:34

Position and motion detection functions:

- interrupt can be generated if acceleration is above or below certain value in one or more axis for certain time

- it can be configured in registers INT_GEN_CFG_XL (06h), INT_GEN_THS_X_XL (07h), INT_GEN_THS_Y_XL (08h), INT_GEN_DUR_XL (0Ah)

- there are similar registers for gyroscope

I thinks the Click/double-click recognition is not available in LSM9DS1 and it is mistake in the datasheet but, I will double check it.

Posted on February 27, 2017 at 14:37

I confirm, c

lick/double-click recognition is not available in LSM9DS1.

It is a mistake

 

on the first page of datasheet.