cancel
Showing results for 
Search instead for 
Did you mean: 

Hello guys, plzz does someone use ADC multichannel, i tried and i use 2 temperatur sensors but they dont give same or approximate values ?!?

yousra rachidi
Associate II
Posted on April 11, 2017 at 15:07

Hello guys, plzz does someone use ADC multichannel, i tried and i use 2 temperatur sensors but they dont give same or approximate values ?!?

4 REPLIES 4
Imen.D
ST Employee
Posted on April 11, 2017 at 15:30

Hi

rachidi.yousra

,

There is many ADC examples within STM32Cube firmware package, I would recommend you the ready-use example in the cube package relevant to the device that you are using to understand the principle.

For more clarification your may refer to your reference manual and this

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libraries-expansions/stsw-stm32html

STM32™’s ADC modes and their applications.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
yousra rachidi
Associate II
Posted on April 11, 2017 at 16:18

thanks Imen, i will see the manual

Posted on April 11, 2017 at 17:07

There are hundreds of STM32 parts at this point, you need to be specific about what model/family you are using.

It is also helpful to provide the code that isn't working, it is hard to review things that can't be seen.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
Posted on April 12, 2017 at 00:42

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6rp&d=%2Fa%2F0X0000000bww%2FCoUnhTtrS25ZTGH1USQYsoYEGB5VZuU8IZ9DDXhEcqM&asPdf=false