2017-03-16 05:19 AM
Hello,
i am trying to use stm32cubemx for a stm32f769-disco board, got a blinky to run with rtos,
but now how do i configure stm32cubemx to get the lcd/touch initialized/running? many thanks for any help!
terter2017-03-16 05:27 PM
1) in your project's Drivers directory make one named BSP
2) in the BSP directory make a directory named STM32F769I-Discovery and a directory named Components
3) copy the board support package from STM32Cube/Repository/STM32Cube_FW_F7_V1.6.0/Drivers/BSP/STM32F769I-Discovery
copy the .h and the .c files for
stm32f769i_discovery
stm32f769i_discovery_lcd
stm32f769i_discovery_sdram
stm32f769i_discovery_ts
copy them into your project's Drivers/BSP/STM32F769I-Discovery directory you made in step 2
4) copy the hardware drivers from STM32Cube/Repository/STM32Cube_FW_F7_V1.6.0/Drivers/BSP/Components
the lcd is an otm8009a so copy the whole directory otm8009a into your project's Drivers/BSP/Components directory
the touch sensor uses the ft6x06 driver so copy that directory as well
either copy the code for the adv7533 or comment it out of stm32f769i_discovery_lcd.h - if you use the hdmi adapter board and not the lcd, thats what this is for
5) add Drivers/BSP/STM32F769I-Discovery to your includes path.
if you're using SW4STM32, select your project, choose properties, c/c++ build, settings, includes
6) add the #includes to your project after the USER CODE BEGIN includes comment
#include 'stm32f769i_discovery.h'
#include 'stm32f769i_discovery_lcd.h'#include 'stm32f769i_discovery_sdram.h'#include 'stm32f769i_discovery_ts.h'7) make a directory at the top level of your project called Utilities, and make a directory inside it called Fonts
😎 copy the fonts from STM32Cube/Repository/STM32Cube_FW_F7_V1.6.0/Utilities/Fonts into your Fonts directory
9) add the initialization calls to your project
uint8_t lcd_status = LCD_OK;
BSP_LCD_Init();
while(lcd_status != LCD_OK);uint32_t ts_status = TS_OK;
ts_status = BSP_TS_Init(BSP_LCD_GetXSize(), BSP_LCD_GetYSize());
that should at least get a person going.
Log in the STM32Cube/Repository/STM32Cube_FW_F7_V1.6.0/Utilities/Log directory is also worth exploring
on edit: i forgot about the rest of the hal drivers
if you didnt add them in stm32cubemx, you'll need to add the hal drivers for
dma2d
dsi
ltdc and ltdc_ex
sdram
stm32f7xx_ll_fmc
copy them from STM32Cube/Repository/STM32Cube_FW_F7_V1.6.0/Drivers/STM32F7xx_HAL_Driver/ into the corresponding Drivers/STM32F7xx_HAL_Driver/ of your project and enable the modules in your project's stm32f7xx_hal_conf.h
2017-03-18 09:36 AM
Thank You so much,
i putted all the things together, to get it compiled i had to exclude the /Utilities/Fonts directory from build (would give multiple references to fontsXX.o)
and add the BSP/Components/Common directory
when i run it the backlite of the lcd is switched on but
BSP_LCD_Clear(LCD_COLOR_LIGHTGREEN);
changes nothing and it crashes writing:
BSP_LCD_DisplayStringAtLine(8, (uint8_t*)'testttest42');
could there be a problem with the initializion from the stm32cubemx?
Initialize all peripherals with their default mode is checked
DMA2D is activated
DSIHost is set to Adapted command mode with TE Pin
SDRAM1 SDCKE0+SDNE0
4 Banks 13bit Addesses 32 Bit Data
LTDC is set to RGB888 DSI-Mode
HCLK is 192MHz
PLL DSI gives 250MHz set back to default 500MHz, no change
DSI txclkesc is 7.8125 MHz set back to default 15.625Mhz, no change
DSI Lane Byte 31.25 MHz set back to default 62.5Mhz, no change
Configuration:
DSI-Host is set according to Application note AN4860 Adapted Command mode page 126 (set back to Default, no change)
are there any interrupts to set or what can be wrong?
all the best
terter
edit:
after changing the user-code block 2 to
BSP_SDRAM_Init();
HAL_Delay(100);
BSP_LCD_Init();
BSP_LCD_LayerDefaultInit(1, LCD_FB_START_ADDRESS); BSP_LCD_SelectLayer(1);BSP_LCD_DisplayOn();
BSP_LCD_SetBackColor(LCD_COLOR_LIGHTGREEN);uint32_t ts_status = TS_OK;
ts_status = BSP_TS_Init(BSP_LCD_GetXSize(), BSP_LCD_GetYSize());BSP_LCD_Clear(LCD_COLOR_LIGHTGREEN);
BSP_LCD_SetTextColor(LCD_COLOR_RED); BSP_LCD_DisplayStringAtLine(8, (uint8_t*)' testttest42 ');i get now an about 800x10px high strip of flickering 'snow' on top of the lcd...
smells somehow like sync/freq issues, but when i search for timing-related stuff in other projects
i find nothing... are they hidden somewhere?
many thanks for some clarification...
terter
edit: semi-solved
when i comment out this part of the stm32cubeMX generated SystemClock_Config() it works!
but what does that mean?
// PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SPDIFRX|RCC_PERIPHCLK_LTDC
// |RCC_PERIPHCLK_RTC|RCC_PERIPHCLK_USART1 // |RCC_PERIPHCLK_USART6|RCC_PERIPHCLK_UART5 // |RCC_PERIPHCLK_SAI1|RCC_PERIPHCLK_SAI2 // |RCC_PERIPHCLK_I2C1|RCC_PERIPHCLK_I2C4 // |RCC_PERIPHCLK_CLK48|RCC_PERIPHCLK_CEC; // PeriphClkInitStruct.PLLI2S.PLLI2SN = 192; // PeriphClkInitStruct.PLLI2S.PLLI2SP = RCC_PLLP_DIV2; // PeriphClkInitStruct.PLLI2S.PLLI2SR = 2; // PeriphClkInitStruct.PLLI2S.PLLI2SQ = 2; // PeriphClkInitStruct.PLLSAI.PLLSAIN = 384; // PeriphClkInitStruct.PLLSAI.PLLSAIR = 7; // PeriphClkInitStruct.PLLSAI.PLLSAIQ = 8; // PeriphClkInitStruct.PLLSAI.PLLSAIP = RCC_PLLSAIP_DIV2; // PeriphClkInitStruct.PLLI2SDivQ = 1; // PeriphClkInitStruct.PLLSAIDivQ = 1; // PeriphClkInitStruct.PLLSAIDivR = RCC_PLLSAIDIVR_2; // PeriphClkInitStruct.Uart5ClockSelection = RCC_UART5CLKSOURCE_PCLK1; // PeriphClkInitStruct.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1; // PeriphClkInitStruct.I2c4ClockSelection = RCC_I2C4CLKSOURCE_PCLK1; // if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) // { // Error_Handler(); // }many thanks for some clarification...
terter
ps. these STM32F7 Boards are really nice but the software (stm32cubeMX , SW4STM32 ) is like a can of worms, very quirky and
strangely the examples are not even made with stm32cubeMX. remembering having a much smother ride with the NXP1769-Expresso
now to the next
problem
challenge... getting stemwin to run 🙂2018-08-03 01:48 AM
The main problem is the template of the stm32f769-disco board. There are so many wrong values and settings done.
So, the 3 frequencys are importend to get the display runnig.
kind regards
Roger