cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF04Sx - WebServer - HTTP

yoann LBY
Senior
Posted on December 11, 2017 at 18:14

hi,

is it possible to limit a connection to the module with one client?

wifi module is miniAP mode and HTTP server application run with web pages html.

One client connect to the wifi module

+WIND:28:Station Associated:44:85:00:F8:B6:DC:0

and i don't want a second client to connect in the same time of client1.

+WIND:28:Station Associated:08:11:96:9D:5E:D8:0

thks

Yoann

1 ACCEPTED SOLUTION

Accepted Solutions
Posted on December 11, 2017 at 18:33

miniAP embedds a DHCP server. You can set the number of delivered IP addresses (ip_num_clients) to just 1. This way second STA can associate, but will be disassociated while client #1 is still in

View solution in original post

1 REPLY 1
Posted on December 11, 2017 at 18:33

miniAP embedds a DHCP server. You can set the number of delivered IP addresses (ip_num_clients) to just 1. This way second STA can associate, but will be disassociated while client #1 is still in