cancel
Showing results for 
Search instead for 
Did you mean: 

Migrate STM32F401RE to STM32F401RB with STM32CubeExpansion_WIFI_V3.0.2

yoann LBY
Senior
Posted on July 04, 2017 at 14:59

hi,

i work on WIFI module SPWF04SA and SMT32F401RE with STM32CubeExpansion_WIFI_V3.0.2 (app client_Socket + MDK-ARM V5.22.0.0).

i would like to migrate to STM32F401RB on my board but i have some issues! 

Pb1: i migrated RE to RB (source CubeMx V4.21.0)

startup_stm32f401xe.s -> startup_stm32f401xc.s

system_stm32f4xx.c -> new system_stm32f4xx.c

stm32_xx_it.c ->  i keep stm32_xx_it.c

STM32F4xx_HAL_Driver -> new STM32F4xx_HAL_Driver 

option target (stm32F401RETx -> STM32F401RB, Xtal = 84Mhz)

i miss something?

Pb2: i use external clock 8Mhz and code generated with CubeMx doesn't work!

internal clock with HSI works!!

fct SystemClock_Config(): 84Mhz with HSE

RCC_OscInitTypeDef RCC_OscInitStruct;

  RCC_ClkInitTypeDef RCC_ClkInitStruct;

    /**Configure the main internal regulator output voltage

    */

  __HAL_RCC_PWR_CLK_ENABLE();

  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);

    /**Initializes the CPU, AHB and APB busses clocks

    */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

  RCC_OscInitStruct.HSEState = RCC_HSE_ON;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

  RCC_OscInitStruct.PLL.PLLM = 8;

  RCC_OscInitStruct.PLL.PLLN = 336;

  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;

  RCC_OscInitStruct.PLL.PLLQ = 4;

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

    /**Initializes the CPU, AHB and APB busses clocks

    */

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

+ fct SystemCoreClockUpdate();

Pb3: pin RESET PA8 to PC12 locked. i modified fct wifi_reset() declaration of pin wifi_instances_t wifi_instances; by GPIO_InitTypeDef  RESET_InitStruct; to configure correctly pin RESET to PC12. Why configuration PC12 is locked (locked to PAx)

Pb4: uart +Dma doesn't work with migration re to rb. stm32 doesn't see communication on uart bus with wifi module (no +WIND scan)

Mridupawan Das, please help....

thks

Yoann

1 REPLY 1
yoann LBY
Senior
Posted on August 01, 2017 at 09:24

Nobody can help me?