cancel
Showing results for 
Search instead for 
Did you mean: 

How can I use Motor Profiler with STEVAL-SPIN3201?

Dror Laor
Associate
Posted on March 20, 2017 at 15:10

I noticed that STEVAL-SPIN3201 is not on the supported boards list for Motor Profiler. Is there an update/path?

2 REPLIES 2
Enrico Poli
ST Employee
Posted on March 22, 2017 at 10:28

Unfortunately the Motor Profiler does not support the STM32 embedded into the STSPIN32F0 System-in-package.

In any case, you can use the Motor Profiler using one of the supported boards and then 'export' the results on the STEVAL-SPIN3201 using the MC Workbench 

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards