cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1 - Multiple ROI Issues

Itamar Eliakim
Associate III
Posted on March 13, 2018 at 13:41

Hi.

At the MWC 2018, ST presented a demo with RGB camera and the VL53L1x with multiple measurement points on the live image

.

I got the evaluation boards this week, the datasheet and API manuals online for this device don’t have enough details how to operate this configuration for multiple ROI

,

I tried to work through this using the example code but the results does make any sense, the distance measurement seems to be correct but it’s similar on all of the pixels within the aperture even when I cover just half of the sensor

.

Did someone succeed operating the ROI to sense the distance in specific pixel within the aperture?

I've developed a small test app for the multiple ROI, here i'm covering half of the sensor, as you can see all pixels returns around the same result:

0690X00000609ykQAA.png

Thanks

,

Itamar

4 REPLIES 4
albagir themut
Associate II
Posted on March 23, 2018 at 13:21

Same issue for me using multiple ROIs. Maybe someone could post some small code how to obtain the correct range value for the whole FoV (13*13 array, one ranging value per item). 

BR,

Albagir

John Tukash
Associate
Posted on May 08, 2018 at 13:33

Yes, I can confirm that on my side I have the same problem and don't know how to solve this issue.

albagir themut
Associate II
Posted on May 17, 2018 at 16:05

Anyone who solved the issue and can provide some code?

John E KVAM
ST Employee
Posted on May 24, 2018 at 23:59

Itamar -

Looking at your data, you didn't 'cover half the sensor'. Despite the rather large IR filter, the hole in the sensor is REALLY small.

I tried this experiment.

I placed my sensor in the bottom of an open box looking up.

This allows me to carefully place my targets. I used a ruler as a target.

I used a box 20cm on a side and 13cm tall. But the dimensions aren't really important.

I marked the centerline and +/- 12.5 degrees.

This allows me to move targets in and out of the Field of View (FoV) repeatably. The ruler simply rests on the sides of the box.

Code follows:

void AutonomousLowPowerRangingTest(void)

{

            uint32_t pMeasurementTimingBudgetMicroSeconds;

            VL53L1_UserRoi_t Roi;

            static VL53L1_RangingMeasurementData_t RangingData;

            printf('Autonomous Ranging Test\n');

            status = VL53L1_WaitDeviceBooted(Dev);

            status += VL53L1_DataInit(Dev);

            status += VL53L1_StaticInit(Dev);

            status += VL53L1_SetPresetMode(Dev,VL53L1_PRESETMODE_LOWPOWER_AUTONOMOUS);

            status += VL53L1_SetDistanceMode(Dev, VL53L1_DISTANCEMODE_LONG);

            status += VL53L1_SetMeasurementTimingBudgetMicroSeconds(Dev,20000); // 8 ms

            status += VL53L1_SetInterMeasurementPeriodMilliSeconds(Dev, 100);

            status += VL53L1_GetMeasurementTimingBudgetMicroSeconds(Dev, &pMeasurementTimingBudgetMicroSeconds);

            printf('Timing Budget = %d\n', pMeasurementTimingBudgetMicroSeconds);

            Roi.TopLeftX = 0;

            Roi.TopLeftY = 15;

            Roi.BotRightX = 15;

            Roi.BotRightY = 0;

#if 1

            Roi.TopLeftX = 5;

            Roi.TopLeftY = 15;

            Roi.BotRightX = 10;

            Roi.BotRightY = 0;

#endif

            status += VL53L1_SetUserROI( Dev, &Roi);

            status += VL53L1_StartMeasurement(Dev);

            if(status){

                        printf('YOU DID SOMETHING WRONG \n');

                        while(1);

            }          

           

                        do // interrupt mode

                        {

                                    __WFI(); // Wait For Interrupt - you could also poll

                                    if(IntCount !=0 ){

                                                IntCount=0;

                                                status = VL53L1_GetRangingMeasurementData(Dev, &RangingData);

                                                if(status==0){

                                                            printf('%d,%d,%.2f,%.2f,%d\n', RangingData.RangeStatus,RangingData.RangeMilliMeter,

                                                                        RangingData.SignalRateRtnMegaCps/65536.0,RangingData.AmbientRateRtnMegaCps/65336.0,HAL_GetTick());

                                                }

                                                status = VL53L1_ClearInterruptAndStartMeasurement(Dev);

                                    }

                        }

                        while(1);

One issue I had was understanding the co-ordinate system.

Assume the (0,0) location is in the bottom left of the chip. (15,15) is in the upper right.

Then view the EVK so the USB is at the ‘top’ and the characters are right-side-up.

Run the code using the (0,15) (15,0) FoV. Move your rulers in an out until you are convinced you are at the edge of the FoV. Mark the box with these edges.

Then run the code using the (5,15) (10,0) FoV. Again move the rulers in an out until you are convinced the FoV has moved “in�?.

 I get a pretty significant change in the ROI. It's about what I would expect.

My only worry is that an ROI change might not change immediately. If a range has started, it might only take effect after the range finishes.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.