cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Flash Loader Demonstrator - Support for STM32F72X

Alex Chen
Associate II
Posted on March 23, 2017 at 08:23

Hi everyone,

I was trying to download firmware in system memory mode via USART using the STM Flash Loader Demonstrator (version 2.8.0). However, there is no '.STMap' memory map file for STM32F722RE/ZE.

Could 

anyone provide the STMap for

STM32F72x family or tell me how to modify through an existing STMap file (like STM32F7_4x_5x_1024K.STmap for example). I don't know what values should be filled in items like PacketSize, ACKVAL.

Thank you.

1 REPLY 1
mn
Associate III
Posted on June 22, 2017 at 09:32

Hi

I am using STM32F746BG and change STmap file as:

[Product]

Name=STM32F7_46_1024K_RAM

PID=0449

BID=1FF0EDBE

FlashSize=0400    ;;ADDR_FLASH_SIZE=FFFFFFFF;  TO BE DONE !!!!

PacketSize=80

ACKVAL=79

MAPNAME=Sectors

PagesPerSector=1

family = 6;

;; InternalRAM

[InternalRAM]

Name=userRAM

Address=20010000

Size=0001D000

Type=111

UFO=111

you can use AN4852 for more

details

.