cancel
Showing results for 
Search instead for 
Did you mean: 

SensorTile Current Comsumption

Zt Liu
Senior III
Posted on September 19, 2017 at 05:44

Hey!

I am currently having fun with Sensortile.

I'd like to know is there any current consumption profile?

(STLCR01V1 already put it into the little box)

I only know that while is connected through the app, 

battery profile tells that it's discharding with about 15mA.

If I turned off the usb debug function, it draws about 10mA.

I would like to know:

1 Can I further reduce the current consumption with all sensors on?

2 In advertising, how much current it take? Can I further reduce it?

   If so, how? Where is the code that I can change the cycle of advertising?

Thanks for reading this post!

Zt.

#stm32l476 #mems #sensortile #bluenrg
0 REPLIES 0