cancel
Showing results for 
Search instead for 
Did you mean: 

Keil IDE: This target device does not support conditional breakpoints

William chang
Associate III
Posted on February 11, 2018 at 01:36

0690X00000609RqQAI.png

here is my conditional breakpoints settings

0690X00000609d2QAA.png

I took exercise as <apnt_230.pdf> did at page 11, 15) watchpoints: Conditional Breakpoints.

The application can use conditional breakpoints. Why I can't? I got a dialogue saying that My 

target device dose not support conditional breakpoints!

Actually, I am using the STMF407 Discovery board as the 

<apnt_230.pdf> using.

So, why? 

Turvey.Clive.002

http://userbadge

 

#conditional-breakpoints
1 ACCEPTED SOLUTION

Accepted Solutions
William chang
Associate III
Posted on February 11, 2018 at 10:21

0690X00000609fgQAA.png

Finally, I found I forget to check the box of Read and Write.

Turvey.Clive.002

‌ Don't tell Bob boys, I make a stupid mistake. ^ ^

His notes is very helpful to get the uVision debugger working, and act like a professional.

View solution in original post

5 REPLIES 5
Posted on February 11, 2018 at 03:37

Not really functionality I use. You might want to check the state of the SB12 solder bridge, and the specific version of the board and ST-LINK firmware. Bob Boys the author of the app note is an occasional visitor here, I will share the post.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
Posted on February 11, 2018 at 04:06

SB12 is connected as default.

My ST-LINK firmware updated recently. Version: V2.J29.S0

Here is my KEIL IDE details:

0690X00000609fbQAA.png
William chang
Associate III
Posted on February 11, 2018 at 10:21

0690X00000609fgQAA.png

Finally, I found I forget to check the box of Read and Write.

Turvey.Clive.002

‌ Don't tell Bob boys, I make a stupid mistake. ^ ^

His notes is very helpful to get the uVision debugger working, and act like a professional.

Posted on February 13, 2018 at 18:35

Hello

I noticed this and by the time I got to answer - you had already found the problem.

You are not the first to forget this - I think there are three others over the years.

So I updated the appnote a bit.  It is now on the Keil website.

Bob

Bob Boys
Senior
Posted on February 20, 2018 at 20:35

Hello

I updated Appnote 230 and it is now on www.keil.com:: 

http://www.keil.com/appnotes/docs/apnt_230.asp

You can adapt this document to many other ST boards.

There have been many improvements and additions to uVision since the last version of this document.

Event Recorder, ULINKplus Power Measurement, FreeRTOS support, ETM trace features and so on....

Thanks

Bob

San Jose, California