cancel
Showing results for 
Search instead for 
Did you mean: 

SP5 Studio 5.5 Problem (CAN Issue)

guo qiang
Senior
Posted on August 10, 2017 at 04:32

1.The CANConfig structure adds a number of field information,it have a ''fifo_rx_callback'' function point.

. Why is there a dialog box in SP5Studio that does not configure fifo_rx_callback?Causes the '' fifo_rx_callback'' function point to NULL

0690X00000607lhQAA.png

2. Building failed when disenable CAN filter.

0690X00000607kVQAQ.png0690X00000607n9QAA.png

this is a bug

Yvin.Erwan.001

‌

erwan.leray@st.com

‌

simon.scullion

‌

null
1 ACCEPTED SOLUTION

Accepted Solutions
procolo
Senior
Posted on August 10, 2017 at 09:46

Hi,

Regarding point 1)

Currently the FIFO is supported only on Pictus and it's going to be introduced in other platforms. You are using bolero B platform so you cannot see FIFO configurator yet but the driver already support it. In the next version FIFO configurator will be available also for your platform.

Reagrding point 2)

As already said, an ER is opened and issue will be solved in next release . Meanwhile, please change can_lld.c file with the attached one.

Best Regards,

Procolo

________________

Attachments :

can_lld.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyWR&d=%2Fa%2F0X0000000b90%2F2JWzlKWEpnxPqdzZyUBe8UFXq4G885aYzSeKIB0n8Gw&asPdf=false

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee
Posted on August 10, 2017 at 09:31

Hello Guo ,

i am submitting an ER (Error Report) for this issue

       Best regards

                   Erwan

procolo
Senior
Posted on August 10, 2017 at 09:46

Hi,

Regarding point 1)

Currently the FIFO is supported only on Pictus and it's going to be introduced in other platforms. You are using bolero B platform so you cannot see FIFO configurator yet but the driver already support it. In the next version FIFO configurator will be available also for your platform.

Reagrding point 2)

As already said, an ER is opened and issue will be solved in next release . Meanwhile, please change can_lld.c file with the attached one.

Best Regards,

Procolo

________________

Attachments :

can_lld.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyWR&d=%2Fa%2F0X0000000b90%2F2JWzlKWEpnxPqdzZyUBe8UFXq4G885aYzSeKIB0n8Gw&asPdf=false