2017-04-22 05:47 PM
Hello!
I want to control ILI9341(SPI LCD) by STM32F103C8.
Simple SPI access is ok.
Most example are belong arduino in internet, but I am using EWARM.
Please share your experience to me.
BR
LC
2017-04-22 06:17 PM
Googling STM32 ILI9341 dumped a bunch of hits
2017-04-24 08:14 PM
Thanks Clive One.
2017-04-29 02:37 AM
Hi ALL
with ILI9341 it has command & data information via SPI interface.
Are they using same SPI function(push data) and necessary to handle the D/C(Data/Command) pin by myself?
In ILI9341 data sheet, there have 9-bit interface.
I think it like I2C style, one more bit indicate the following data either data or command.
Shall we implement it in STM32?
Please let me know your comment.
LC
________________ Attachments : ILI9341.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hygv&d=%2Fa%2F0X0000000bAz%2FcixjhTg0VdSF3Ynh8TvFjjxpjNRiGkPKjCJBO8XIJFA&asPdf=false2017-04-29 03:28 AM
There should be also a 8 bit with dedicated pin for command/data.
For STM32F103, the HW supports 8 or 16 bit bitblock transfer. Extra bit done by SW bit banging?
For newer STM32 with FIFO'd SPI, the HW supports 4,5,6...16 bits so the 9 bit mode seems a better fit, and save a pin.