2018-04-02 04:08 AM
As the title suggests, I want to modify the HAL I2C library so that after a transmit (HAL_FMPI2C_Master_Transmit), it will not generate a STOP.
I think I have to modify the file stm32f4xx_hal_fmpi2c.c but I have not been successful.
In order to receive data from an I2C device, I first have to send some commands to it. Using the mem_read() function is not an option, as I need to send more than just the location in memory where I want to read. Anyone who can point me in the right location? I tried to replace the 'AUTOEND' with 'SOFTEND' but I think this is not sufficient. Thank you!