cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo/Discovery ST-Link Clears Automatically Clears Flash on USB connection

_ Anyland
Associate II
Posted on April 26, 2017 at 16:10

Why does the Nucleo/Discovery onboard ST-Link clear flash memory (0x08000000 - 0x08000200) when I connect to the ST-Link USB?

I've had this happen on multiple boards, and can watch it do this from the ST-Link Utility program.

5 REPLIES 5
_ Anyland
Associate II
Posted on April 26, 2017 at 16:45

Fixed: ST-Link firmware needed updating.

AvaTar
Lead
Posted on April 26, 2017 at 18:26

I never experienced such an issue with my (admittedly older) Nucleo boards.

It would be helpful for others if you name the board(s) and the SW version you had that trouble with.

_ Anyland
Associate II
Posted on April 26, 2017 at 19:12

I've had the issue on the STM32L053 Discovery, Nucleo-L053R8, and the Nucleo-F411RE. I already updated the firmware, so I'm can't check with 100% certainty, but I believe I had both v2.23 and v2.22 of the firmware causing issues. Updating to v2.28.18 fixed the problem.

Posted on April 26, 2017 at 20:28

There has been a lot of tinkering with the mbed firmware, especially the faux MSC and holding devices in reset. The last batch of STM32F4-DISC1 boards wouldn't run from charger cables until updated. The early V2.2x would make sense.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
Posted on April 27, 2017 at 07:24

My latest Nucleo is a 746ZG from last year, which doesn't have >this< issue.

It exhibits another problem (The Cortex M7 debug problem), so I re-flashed the onboard ST-Link into a JLink.