cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH accelerometer single&double click interrupt problem

Donald Chen
Associate II
Posted on May 23, 2017 at 06:01

Hey guys, I am doing single and double click interrupt generate for LIS3DH accelerometer. I have a question, it is possible single click will generate interrupt when set both single&double click. I found out the accelerometer will only generate interrupt when I tap on the accelerometer twice. So, it is possible to generate interrupt when I tap the accelerometer only once? I have a function to handle interrupt, it will only generate interrupt when I tap it twice. Izzit normal?

#accelerometer
0 REPLIES 0