2018-01-07 11:05 PM
Hello,
I did USB VCP CDC FS code in STM32F405.
I works fine.i tested it with terminal software.
Now i want to test same with .NET C♯ application software (with USB protocol only).
But unfortunately USB is not detected in .net c♯ application.
Anybody have some example code for same?@
OR
Any solution for same so i can proceed with my target.
Thank you.
Turvey.Clive.002
null2018-01-08 01:31 AM
If you are using the CDC class with Windows, the USB interface is bound to the USB serial driver by default. This means that you can only interact with it as a Serial COM Port, in .NET you have the System.IO.Ports.SerialPort class for that. If you are trying to access this interface with a native USB application (such as LibUsbDotNet), you have to uninstall the serial driver from the USB interface, and set the WinUSB driver for it.
2018-01-08 02:26 AM
Thank you.
I did this i uninstalled serial drivers and installed WinUSB Drivers but problem still persist.
Apart from WinUSB drivers what extra should i need for my C#.Net Application programming?
Basically i want STM32F405 to PC base Application software(Developed in C#.Net)communication.
2018-01-08 04:03 AM
If you can observe the WinUSB interface in Device Manager then the problem is most likely in your application. It's hard to say anything without any code attached - and this is not the proper forum for .NET USB application development - but I would consider trying all alternative ways of detecting the device, e.g. VID-PID based discovery.
2018-01-08 07:24 AM