cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 Maximum input Frequency

Oktay TURK
Associate II
Posted on April 28, 2018 at 19:09

I use STM32F103 how much is the maximum input maximum encoder frequency. For example if the possible i reading the 20 KHz. I use the TIMER4 encoder mode but i not read the up the 2 KHz. How much is the maximum frequency value?

1 REPLY 1
Posted on April 28, 2018 at 20:14

The TIM's should work into the MHz, but don't expect to interrupt at such high rates.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..