cancel
Showing results for 
Search instead for 
Did you mean: 

Receive in Canbus

Pedram
Associate III
Posted on January 01, 2018 at 22:29

aHello friends ,

I have a few questions about Receive in Canbus 

if i want Receive message with interruption I must use HAL_CAN_Receive_IT  

How can i Be aware of the existence of a new message ? 

How can i set device ID ?

2 REPLIES 2
T J
Lead
Posted on January 01, 2018 at 23:00

I started by using a CanDo unit from the UK.

I made that unit transmit every 10mS, then I worked on my receiver.

do you have a commercial unit like that for testing ?

Posted on January 02, 2018 at 03:19

I've got a Ginkgo USB-Can Adapter which can send packets manually or automatically.  There is no 'device ID'.  You need to setup the receive ID and mask to configure the device to receive a specific packet ID or IDs.  I just learned this as well.