2017-05-19 08:25 AM
Hi!
When I flash a .hex or .bin file with a ST-LINK V2 device on my STM32F4 microcontroller (with ST-LINK utility), the program only works if both the ST-LINK V2 and my MCU board stay connected to the computer (through a USB cable). Whenever I unplug one of them the program just flashed on the board does not run anymore.
Does anyone have any idea of what is happening ?
Thanks for your help!
#st-link #flash-stm32 #st-link-utilitySolved! Go to Solution.
2017-05-22 04:46 AM
Thank you both of you but I managed to solve the problem.
It was actually due to the ST-Link device that was still plug to the MCU board and keeping it from running the program (even though it wasn't plug to the computer and not powered on...)
2017-05-19 08:45 AM
Hi
baures.tim
,ease refer tothis application note to verifyyour hardware implementation:
-Nesrine-
2017-05-19 11:07 AM
2017-05-22 04:46 AM
Thank you both of you but I managed to solve the problem.
It was actually due to the ST-Link device that was still plug to the MCU board and keeping it from running the program (even though it wasn't plug to the computer and not powered on...)