cancel
Showing results for 
Search instead for 
Did you mean: 

Is nucleo_l152re a two layer (or more) PCB design?

Posted on December 14, 2017 at 18:57

I see there some have problems (the board doesn't work well anymore) after separating the programmer part from the rest of the board. And I intend to use this tool to cut the bridges...

0690X0000060PGVQA2.jpg

#pcb #cut #bridges
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on December 14, 2017 at 19:06

Load the Gerbers into a viewer?

http://www.st.com/resource/en/board_manufacturing_specification/nucleo_64pins_gerber.zip

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2
Posted on December 14, 2017 at 19:06

Load the Gerbers into a viewer?

http://www.st.com/resource/en/board_manufacturing_specification/nucleo_64pins_gerber.zip

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on December 14, 2017 at 19:20

So two layers... thank you Clive! There may be several chances to have bridged traces on the bottom layer on a rough cut, and one for the top layer...

I recommend to make those PCB bridges wider and the traces with more space between them.

Or on the microcontroller board, 0 ohm resistors as a bridge for the signal traces, that can be un(de)-soldered to avoid short circuit after a separation.