cancel
Showing results for 
Search instead for 
Did you mean: 

CCA01M1 with F411RE

Mark Nordstrand
Associate
Posted on June 22, 2017 at 20:07

Using System Workbench and targeting a Nucleo-F411RE.  Set JP5 on the Nucleo board and routed 5V to CN2 to the correct header position.  Grabbed the SOUNDTER1 package and programmed the board.  Not getting any output.

I noted that the project was for a F401RE, and went through generating the initialization code for both the '01 and the '11.  All I really observed was a change in clock and flash latency.  

Is there something else that I'm missing?  Better yet, is there a good outline for what should be changed in the source to switch between either processor in System Workbench?

0 REPLIES 0