cancel
Showing results for 
Search instead for 
Did you mean: 

Measuring VL6180X with close distances

Tobias Nagel
Associate II
Posted on August 16, 2017 at 16:36

Hey,

I am having the VL6180X Satellites sensor for ranging measurements. After connecting it, I receive some measurement values - but they are the wrong ones. The sensor isn't reacting to changes in a distance between 0mm and ~50mm. It keeps showing me the value '4 mm'. Beyond that distance of 50 mm, the values start increasing, which is fine.

Is there anything I am forgetting? I have set the Offset to 0 mm. The range-ignore features and the early convergence are disabled (by register 0x02D). I performed the measurements in the darkness.

Thanks in advance!

#close-measurement #vl6180x
1 REPLY 1
John E KVAM
ST Employee
Posted on January 02, 2018 at 17:45

At close distances the VL53L0 has a bit of a blind spot. The light from the laser hits bounces between the target and the material the sensor is mounted on. This 'multipath' means the reported distance starts increasing as the target gets very close. If you can guarantee the actual distance never gets closer than 1.5cm, the result is accurate. But below 1.5cm there is an issue.

Our solution is to back the sensor up in some sort of cavity to guarantee the real target cannot get too close.

- john


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.