cancel
Showing results for 
Search instead for 
Did you mean: 

FLASH-USART-FLASH (Circular)

knight master
Associate II
Posted on July 02, 2017 at 16:30

FLASH-USART-FLASH  (Circular)

hallo guys ,

I have one assignment ,

that i have to read array of data from FLASH memory and send it through the USART  after that I have to send array of data through DOCKLITE and store it in FLASH  and when i  remove and plug in again the what ever array of data is in FLASH i have send through USART .

flow is  1. read array from FLASH

2.send through USART to DOCKLITE-

3.NOW DOCKLITE send data one by one

4. store in data in FLASH 

5. READ array from FLASH

guys any idea how to do it ...

1 REPLY 1
Posted on July 02, 2017 at 17:21

Start with the elements of the problem you understand how to implement, or do mostly, and then extend and expand from there.

Discuss with the person setting the assignment.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..