cancel
Showing results for 
Search instead for 
Did you mean: 

smps parallel connection

ibrahim etem
Associate
Posted on July 19, 2017 at 12:15

Hello. i design L6566BH on design süite. But i see that max power out is 350w. if i do same smps 3 pieces and i want to get 1050w can i connect their outputs in parallel connection? because i see that it is not basic thing. one smps gives 10A the other give 2A  for this i want they share current value equal. for example i need 30A. and i want 10a/smps give power

is there a way or is there a calculator half or full bridge?

thanks

0 REPLIES 0