cancel
Showing results for 
Search instead for 
Did you mean: 

Problem BlueNRG-1 and ST-Link Debugger under Eclipse

Tino Beilken
Associate II
Posted on July 19, 2017 at 15:28

I have the STEVAL-IDB007V1 DK with the BlueNRG-1 chip.

First I work with IAR Embedded workbench and it works fine.

Today I install Eclipse with the system workbench for STM32 and port the Project for eclipse.

It works fine but the problem is to use the debugger (ST-Link V2) and I don´t know why.

I have install the openocd for GNU ARM Eclipse and add it to the Debug Configuration.

But every time I start debugging, I get the failure 'Error while launching command: gdb -- version

Have anyone an idea ?

In the Debug Configuration which Config options the BlueNRG-1 Chip needed ?

0 REPLIES 0