cancel
Showing results for 
Search instead for 
Did you mean: 

Issue wtih FIFO threshold and SPI working

Posted on October 03, 2017 at 15:42

Hi 

    I hooked up two STM32L432 nucleo boards in master-salve mode of SPI. I am setting up DMA and SPI with 8 bit (BYTE) boundary and data width.  If I set the FRXTH threshold  for SPI  as LL_SPI_RX_FIFO_TH_HALF the slave DMAs dont get transfer completes both for Tx and Rx. I found by toggling GPIOs in the call back functions for both RX and TX. But if I do set the treshold as  LL_SPI_RX_FIFO_TH_QUARTER I see everything is fine... My question is do these thresholds have anything to do with the data size settings???... Thanks.

Regards

Bala

0 REPLIES 0