2017-09-07 12:53 PM
Hi. I am trying to perform i2c communication between a stm32f429 discovery board and an arduino mega adk. The stm board is the master transmitter and the arduino is the slave receiver. Currently, nothing is printed on the arduino serial monitor. I am using the example code for slave receiver for the arduino. Any help would be greatly appreciated.
void scl_pin()
{ RCC ->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; GPIOB ->MODER |= GPIO_MODER_MODER6_1; GPIOB ->AFR[0] = GPIO_AF4_I2C1<<24;}void sda_pin(){ RCC ->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; GPIOB ->MODER |= GPIO_MODER_MODER7_1; GPIOB ->OTYPER |= GPIO_OTYPER_OT_7; GPIOB ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR7_1; GPIOB ->PUPDR |= GPIO_PUPDR_PUPDR7_0; GPIOB ->AFR[0] = GPIO_AF4_I2C1<<28;}void i2c_setup(){// uint16_t freqrange = 0;
// uint16_t pclk1 = 0;// pclk1 = RCC_CLOCKS.PCLK1_Frequency;// freqrange = (uint16_t)(pclk1 / 1000000); uint32_t frequency = 0; uint32_t read_reg = 0; frequency = SystemCoreClock; I2C1 ->CR2 |= I2C_CR2_FREQ_4; I2C1 ->CCR |= 0x50; I2C1 ->TRISE = 0x11; I2C1->CR1 |= I2C_CR1_ACK; I2C1 ->CR1 |= I2C_CR1_PE;I2C1 ->CR1 |= I2C_CR1_START;
read_reg = I2C1->SR1; I2C1->DR = 0x08; read_reg = I2C1->SR1; read_reg = I2C1->SR2;}void send_data(uint8_t data)
{// while(!(I2C1->SR1 & I2C_SR1_TXE)) I2C1 ->DR = data;}int main(void){ i2c_enable(); led_init1(); led_init2(); scl_pin(); sda_pin(); i2c_setup();// if(I2C1->CR1 & I2C_CR1_ACK)// GPIOG ->BSRRL |= GPIO_BSRR_BS_13; while(1) { send_data(5); }}I have only posted the code relevant to i2c.
For arduino:
&sharpinclude <Wire.h>
void setup() {
Wire.begin(8); // join i2c bus with address &sharp8 Wire.onReceive(receiveEvent); // register event Serial.begin(9600); // start serial for output}void loop() {
Serial.print('Entered Loop'); delay(100); // print the integer}void receiveEvent(int howMany) {
while (1 < Wire.available()) { char c = Wire.read(); // receive byte as a character Serial.print(c); // print the character }}Thanks
#stm32f429 #mega-adk #i2c #arduino2017-09-07 02:28 PM