cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt and wakeup pins configuration SPC560B

AVINASH PULI
Associate
Posted on September 22, 2017 at 06:51

hi everyone ,

I am using SPC560B discovery board , I am new to spc5 studio ,could someone help me  how to configure the WAKEUP PINS  to wakeup the MCU from STOP mode . My requirement is the MCU should identify the wakeup happens by which pin exactly kindly someone help on this issue,

My application is to wakeup the MCU from GSM RI interrupt pin and also when the MCU is running mode it should get interrupt from RI pin.
1 REPLY 1
Erwan YVIN
ST Employee
Posted on September 25, 2017 at 11:13

Hello Avinash Puli ,

There are some examples 

how to use the WKUP Interrupts in this following application (Cf Application Wizard)

SPC560Dxx OS-Less WKPU LPM Test Application for Discovery

   Best regards

               Erwan