cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F107 UART Interrupt issue with HAL

Buelent Cakir
Associate II
Posted on October 10, 2017 at 00:18

Hi,

I've a question regarding the HAL UART Environment. I could observe that the Interrupt are raised sometimes 2x although  I'm sending only one Byte for the STM32 where I'm reading each single byte.

At which conditions can this happen?

#cube-hal #stm32 #uart-it
1 REPLY 1
Posted on October 10, 2017 at 02:32

Perhaps you can illustrate with some code and diagrams?

Does this occur on a continuous basis, or just when you first initialize the USART?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..