cancel
Showing results for 
Search instead for 
Did you mean: 

Problem communication STM32F405VG and I2C EEPROM (M24M02-DRMN)

Posted on October 26, 2017 at 12:05

Hi all.

We have a lot of problems communicating with one I2C EEPROM (M24M02-DRMN). Many times when we try to write or read we see into HAL functions for reading/sending HAL_BUSY answer. Then, we lost data in our application after power-up.

The interface for epprom is easy, The IC have following pins:

 0690X00000608j4QAA.png

1) We put pin 1,2,4 to ground.

2) Pin A2 is pull-up to 3.3V with one 10k resistor.

3) VCC is 3.3V

4) /WC is tied to GPIO line microcontroller

5) SCL and SDA is i2c bus and they have the pull-up resistor for working bus.

Do you know similar problems.

Thans in advance.

Best regards!

#i2c-problem ##hal_busy #hal-driver #eeprom
1 REPLY 1
Rafael Alcaide
Associate
Posted on October 30, 2017 at 10:00

This problem seems related with the post

https://community.st.com/0D50X00009XkeulSAB

. Have you try with the last proposed solution?