cancel
Showing results for 
Search instead for 
Did you mean: 

[Bug] [Regression] STM32CubeMX 4.26.0 copies unnecessary files

Morty Morty
Associate III
Posted on July 03, 2018 at 16:24

Since STM32CubeMX 4.26.0 the file 'Drivers/CMSIS/Device/ST/STM32F3xx/Source/Templates/system_stm32f3xx.c' is created, even if 'Copy only the necessary library files' is selected.

#stmcube-bug #regression-testing-overrated #regression #bug
3 REPLIES 3
Houda GHABRI
ST Employee
Posted on July 05, 2018 at 17:17

Hi 

moritz.struebe

,

Thanks for your feedback.

I&39m not able to reproduce this issue: with 4.26.0 and 

&39Copy only the necessary library files&39 selected Drivers/CMSIS/Device/ST/STM32F3xx/Source/Templates is empty.

Could you please send me your ioc?

Regards,

Houda

Posted on July 06, 2018 at 09:06

Sure, though sending does not seem possible using this forum (not even using PM)

https://cloud.redheads.de/index.php/s/Six3AtBXdXfaHYb

You have to regenerate the project until you get a (grammatically wrong) warning that there was a problem generating the 'Makefileproject'. Just press the button multiple times. I assumed the warning was about some locking issue with my IDE, yet after ensuring that it can be reproduced using the striped ioc, it seems purely CubeMX-related to me. The template folder is generated even without the warning, yet is empty.

Houda GHABRI
ST Employee

Hi @Moritz Strübe​ ,

Sorry for the late response.

This issue is already resolved , you can switch to the latest version of STM32CubeMX 4.26.1 or 4.27.0 scheduled for the end of this week.

Best regards,

Houda